Other Parts Discussed in Post: AWR1642, AWR1642BOOST

作者: TI 工程师 Wesley He 

在一些特殊的使用场合,有需要使用AWR1642对PMIC的输出电压进行调节,或是读取PMIC 内部的工作状态,此时需要I2C接口对PMIC进行读写操作,本文介绍了在现有的mmWave SDK demo中集成I2C接口驱动所需的步骤及操作。

本文的测试环境如下:

  • 测试软件版本:mmWave SDK 2.0.0.4
  • 测试硬件:AWR1642BOOST EVM

1.      在mmWave SDK demo中增加I2C驱动代码

第一步是添加代码以包含和初始化I2C驱动程序。从I2C接口发送和接收均需要此驱动程序的支持,以下是在mss_main.c中添加的初始化I2C驱动程序的C代码。此测试代码可以复制到现有工程中。I2C驱动操作步骤为:GPIO初始化,I2C驱动初始化,配置I2C改写PMIC(LP87524B)寄存器以实现PMIC输出电压调节。

注意LP87524B寄存器信息来源于其datasheet:LP87524B/J-Q1具有集成开关的具有集成开关的 4-A + 2.5-A + 两个 1.5-A 降压稳压器 数据表 (Rev. A),I2C驱动参考代码如下:

#include <ti/drivers/i2c/i2c.h>

 

static int32_t I2C_GPIOInit(void)

{

#if (defined(SOC_XWR14XX))

   /* Setup the PINMUX to bring out the XWR14xx I2C pins */

   Pinmux_Set_OverrideCtrl(SOC_XWR14XX_PINR3_PADAH, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);

   Pinmux_Set_FuncSel(SOC_XWR14XX_PINR3_PADAH, SOC_XWR14XX_PINR3_PADAH_I2C_SDA);

   Pinmux_Set_OverrideCtrl(SOC_XWR14XX_PINP4_PADAI, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);

   Pinmux_Set_FuncSel(SOC_XWR14XX_PINP4_PADAI, SOC_XWR14XX_PINP4_PADAI_I2C_SCL);

#else

   /* Setup the PINMUX to bring out the XWR16xx I2C pins */

   Pinmux_Set_OverrideCtrl(SOC_XWR16XX_PINF13_PADAH, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);

   Pinmux_Set_FuncSel(SOC_XWR16XX_PINF13_PADAH, SOC_XWR16XX_PINF13_PADAH_I2C_SDA);

 

   Pinmux_Set_OverrideCtrl(SOC_XWR16XX_PING14_PADAI, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);

   Pinmux_Set_FuncSel(SOC_XWR16XX_PING14_PADAI, SOC_XWR16XX_PING14_PADAI_I2C_SCL);

#endif

   return 0;

}

static int32_t I2C_Communication_Test()

{

   bool           retVal = false;

   int32_t         errCode = 0;

   uint32_t       arg;

   uint8_t                 rxData[16];

   uint8_t                 txData[16];

   I2C_Transaction         i2cTransaction;

   I2C_Handle     i2cHandle;

   I2C_Params     i2cParams;

 

   /* Reset the transmit and receive buffer */

   memset(&rxData, 0, sizeof (rxData));

 

   /* Initializa the I2C driver */

   I2C_init();

 

   /* Initialize the I2C driver default parameters */

   I2C_Params_init(&i2cParams);

 

   i2cParams.transferMode = I2C_MODE_BLOCKING;

   i2cParams.bitRate = I2C_100kHz;

 

   /* Open the I2C driver */

   i2cHandle = I2C_open(0, &i2cParams);

 

   if (i2cHandle == NULL)

   {

       System_printf ("Error: I2C Driver Open failed\n");

       return -1;

   }

 

   /* Configure the I2C device in I2C_CMD_ADDR_MODE mode */

   arg = 0;//arg set to 0, and the I2C addr mode is 7-bit.

   errCode = I2C_control (i2cHandle, I2C_CMD_ADDR_MODE, (void* )&arg);

   if (errCode < 0)

   {

       System_printf ("Error: I2C control Set I2C_CMD_ADDR_MODE failed [Error code %d]\n", errCode);

       return -1;

   }

 

//read the LP87524B buck3 output voltage register

   txData[0] = 0x10;

   i2cTransaction.slaveAddress = 0x60;//LP87524B/J-Q1 Device Address = 0x60

   i2cTransaction.writeBuf = txData;

   i2cTransaction.writeCount = 1;

   i2cTransaction.readBuf = rxData;

   i2cTransaction.readCount = 1;

   retVal = I2C_transfer(i2cHandle, &i2cTransaction);

   if (retVal == false)

   {

       System_printf ("Error: I2C Transfer failed\n");

       return -1;

   }

   System_printf("I2C_READ: addr=0x%x, Val=0x%x\n",txData[0],rxData[0]);

//write the LP87524B buck3 output voltage = 2.0V

   txData[0] = 0x10;

   txData[1] = 0xbb;//default=0xca,2.3V,0xb1=1.8V, 0xbb=2.0V

   i2cTransaction.slaveAddress = 0x60;//LP87524B/J-Q1 Device Address = 0x60

   i2cTransaction.writeBuf = txData;

   i2cTransaction.writeCount = 2;

   i2cTransaction.readBuf = rxData;

   i2cTransaction.readCount = 0;

   retVal = I2C_transfer(i2cHandle, &i2cTransaction);

   if (retVal == false)

   {

       System_printf ("Error: I2C Transfer failed\n");

       return -1;

   }

   System_printf("I2C_Write: LP87524B buck3 = 2.0V Done\n");

 

//read the LP87524B buck3 output voltage register

   txData[0] = 0x10;

   i2cTransaction.slaveAddress = 0x60;//LP87524B/J-Q1 Device Address = 0x60

   i2cTransaction.writeBuf = txData;

   i2cTransaction.writeCount = 1;

   i2cTransaction.readBuf = rxData;

   i2cTransaction.readCount = 1;

   retVal = I2C_transfer(i2cHandle, &i2cTransaction);

   if (retVal == false)

   {

       System_printf ("Error: I2C Transfer failed\n");

       return -1;

   }

   System_printf("I2C_READ: addr=0x%x, Val=0x%x\r\n",txData[0],rxData[0]);

 

//write the LP87524B buck2 output voltage = 1.5V

   txData[0] = 0x0e;

   txData[1] = 0Xa2;//default=0xb1,1.8V, 0x4d=1V 0xa2=1.5V

   i2cTransaction.slaveAddress = 0x60;//LP87524B/J-Q1 Device Address = 0x60

   i2cTransaction.writeBuf = txData;

   i2cTransaction.writeCount = 2;

   i2cTransaction.readBuf = rxData;

   i2cTransaction.readCount = 0;

   retVal = I2C_transfer(i2cHandle, &i2cTransaction);

   if (retVal == false)

   {

       System_printf ("Error: I2C Transfer failed\n");

       return -1;

   }

   System_printf("I2C_Write: LP87524B buck2 = 1.5V Done\n");

   if (retVal == false)

   {

       System_printf ("Error: I2C combined Transfer to Slave failed\n");

       return -1;

   }

   /* Close I2C driver */

   I2C_close(i2cHandle);

   return 0;

}

 

//Call these function in void MmwDemo_mssInitTask(UArg arg0, UArg arg1)

   errCode = I2C_GPIOInit();

                if (errCode == -1)

       System_printf("I2C_GPIOInit Error\r\n");

   errCode = I2C_Communication_Test();

   if (errCode == -1)

       System_printf("I2C_Communication_Test Error\n");

   else

       System_printf("I2C_Communication_Test Done\n");

2.      将工程链接到I2C驱动库

最后一步是通过链接I2C驱动程序来构建可执行文件。 如果使用CCS项目,可以将I2C驱动程序添加到项目的链接器属性中,如图1所示。

图1. CCS Project Linker Properties

 

如果使用makefile编译工程,执行相同的程序。

###################################################################################

# Additional libraries which are required to build the DEMO:

###################################################################################

MSS_MMW_DEMO_STD_LIBS = $(R4F_COMMON_STD_LIB)                                                              \

                                        -llibpinmux_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                           \

                                        -llibdma_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                                                \

                                        -llibcrc_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                                  \

                                        -llibuart_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                                                \

                                        -llibgpio_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                               \

                                        -llibmailbox_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                          \

                                        -llibmmwavelink_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                  \

                                        -llibmmwave_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                       \

                                        -llibcli_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)                                  \

                                        -llibi2c_$(MMWAVE_SDK_DEVICE_TYPE).$(R4F_LIB_EXT)

MSS_MMW_DEMO_LOC_LIBS = $(R4F_COMMON_LOC_LIB)                                                              \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/pinmux/lib                              \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/uart/lib                                    \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/dma/lib                                   \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/crc/lib                                      \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/gpio/lib                                   \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/drivers/mailbox/lib                             \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/control/mmwavelink/lib                     \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/control/mmwave/lib                           \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/utils/cli/lib                                          \

                                   -i$(MMWAVE_SDK_INSTALL_PATH)/ti/utils/i2c/lib

 

3.      运行测试例程

运行测试程序后,CCS控制台输出打印信息如下,使用万用表测量LP87524输出电压即为设置的电压,I2C驱动添加成功。

**********************************************

Debug: Launching the Millimeter Wave Demo

**********************************************

I2C_READ: addr=0x10, Val=0xca

I2C_Write: LP87524B buck3 = 2.0V Done

I2C_READ: addr=0x10, Val=0xbb

I2C_Write: LP87524B buck2 = 1.5V Done

I2C_Communication_Test Done

4.      参考资料

Anonymous