This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解决LMH6502问题

希望有人可以帮到我,上一个帖子好像沉了一样。

问题描述如上一个帖子的最后一条回复,链接如下:

e2echina.ti.com/.../489149

  • 还在那个帖子下面继续补充, 可以再把那个帖子拉起来.

    我看那个帖子已经很多回复, 可以把最新问题整理一下, 重新发一帖, 免得让大家用很多时间去看帖子, 也不知从哪里讲

  • 您好,

    VG的值受供电电压的影响。当供电电压为5V(V+ - V-)时,1是VG的范围小了,2是最大增益也减小了,3是高频响应也受到影响。具体参考数据手册20页OPERATING AT LOWER SUPPLY VOLTAGES。

    当供电电压为5V(V+ - V-)时,可以参照数据手册Figure 35设定VG值,VG≤1.1V。

  • 很感谢您提供的信息,文档中的大致意思我是理解了,但还是不明白减小了V+后,VG_LIMIT是如何减小的。
    就像文档中举得例子,for example, with V+ = 2V, and V− = −3V, VG_LIMIT = 0.40V which results in maximum gain being
    2.5dB less than what would be expected when VS is higher.
    为什么在这种情况下VG_LIMIT = 0.40V?