This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ40Z50 chem_ID的问题

Other Parts Discussed in Thread: BQSTUDIO

各位大神,大家好

1.刚做的chem_ID , report返回的ID是400,但是DOD error是小于15%,如附件。

现在选用了400的ID导入后跑循环,SOC基本上准了,但是FCC一直比电池实际容量小,

0.1C放电到SOC为0后还可以放大概1个小时左右才会保护,请问是不是还是chem_ID做的有问题。

2.按资料上说的做chem_ID是要电池充饱搁置2小时再0.1C放电到2.8V保护,请问这个2.8V是针对三元电池的吗?

我在做chem_ID时是放电到2.5V保护的,因为我们的电池是磷酸铁锂的,这样有关系吗?

以上请大家帮忙看下