This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936采用同步模式,DS90UB935也采用同步模式,总是不能锁定

请教:DS90UB936采用同步模式,DS90UB935也采用同步模式,总是不能锁定。936采用非同步模式时正常,不知为什么?

  • 请问在工作和不工作时, DS90UB936和DS90UB935上的MODE pin配置是怎样的?
    他们是否改变了寄存器值?
  • 1、同步模式下不能LOCK,936 MODE PIN配置如下:

    935 MODE PIN配置如下:

    2、在以上同步模式不能锁定的情况下,将936的0X58寄存器更改为0X5A(936工作在非同步模式),此时935不作任何变化,935与936可以LOCK,并且LOCK稳定。

    3、在1、2的基础上,通过修改935的0X30寄存器,更改为0X4A(935也工作在非同步模式),此时935与936也可以LOCK,并且LOCK很稳定,读写前端SENSOR也正常,视频传输出正常。

    总结:两端在非同步模式下,可以正常LOCK,正常传输视频。在同步模式下,不能LOCK,请指点,给出建议,谢谢!

  • 请不要更改寄存器0x30和0x4A。

    在同步模式下,建议您在936上编写以下序列:
    1)在寄存器0x4C中选择正确的Rx端口。 如果使用端口0,则写入0x01。
    2)寄存器0x58应设置为值0x5E。
    3)0x6D的值应为0x7C