This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594输出2GHz杂散信号

Other Parts Discussed in Thread: LMX2594

LMX2594配置:

参考信号:100MHz LVDS

输出信号:13.1GHz

PFD:200MHz

RFoutA输出有2GHz的杂散信号,幅度为-42dBm左右。

更改RFoutA的输出频率分别为7.1GHz/9.1GHz/11.1GHz,输出2GHz的杂散信号不移动。

并且输出7.1GHz时,2GHz的杂散信号为-24dBm.

LMX2594的供电为:12V---集成电感的DC-DC---3.6V----LDO TPS74801---3.3V

DC-DC的开关频率分别设置为1MHz/2MHz,在上述4种配置情况下,2GHz杂散信号仍然存在.

从外部给LMX2594直接供3.3V,在上述4种配置情况下的2GHz杂散信号消失。

初步怀疑是DC-DC的开关频率影响了输出杂散

请问:

1.2MHzDC-DC的开关频率是如何经过LMX2594后变成2GHz杂散?

2.在当情情况下如何消除或者减少输出的2GHz杂散信号?

多谢!