M-BUS电路调试过程中,应用TSS721芯片数据手册中的光电耦合电路,主机连接PC端,430单片机的串口连接TSS721芯片作为从机。通过PC端给TSS721发送数据,PC端收发的数据正常,但是用示波器在TSS721的TX端查看波形会发现,TSS721的TX引脚发射数据之后,会继续发送TSS721的RXI引脚收到430单片串口TX的数据,想咨询一下怎么把后面收到的数据屏蔽不再通过TSS721的TX引脚发射?
查看TSS721芯片数据手册的page4发现,它已经说明RX收到的会发送到TX货TXI引脚,会产生数据冲突,这个该怎么处理?调整RIS的电阻值,甚至直接连接地都不能去掉。