This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ32000后备电池的供电问题

Other Parts Discussed in Thread: BQ32000

        我的BQ32000后备电池是用3.0V-3.3F的超级电容实现的,但是发现电压低于2.8V的情况下切换到Vbackup的时候测试得到超级电容输出的电流是70uA左右,这个电流正常么,不是说后备电池供电的情况下功耗2uA吗?为什么不是这样的呢,还是需要用代码进行操作呢?请群里面的大侠指导一下哦!

  • 您好,

    这个电流是正常的,可参考数据手册中6.7 Typical Characteristics中Figure 2曲线图。
  • 多谢,您的回答,也就说在单独Vbackup供电的情况下,最小输出电流就是70uA才能保证芯片在主电源掉电的情况下正常计时是吧?有没有什么操作方式能够在单独Vbackup供电的情况下可以减小输出电流,达到较长时间断开主电源还能够保持时间的作用呢,比如保持一周正常计时,谢谢
  • 您好!数据手册6.5小节里面提到 Ibackup 最大1.5uA,但是有需要VCC一个1ms的脉冲,这是什么意思,既然主电源都已经掉电了怎么实现这个脉冲呢,还是在掉电前就这样做,将RTC的后备电池电流降低呢,这样是不是就需要控制RTC的VCC供电引脚了呢?谢谢!
  • 您好,看下8.2.2.3 Utilizing the Backup Supply,我的理解是VCC切换到BACK电压时,需要立即给VCC管脚一个0-VCC的1ms宽度的脉冲电压,芯片 Ibackup才能耗电最大1.5uA。
    这应该是芯片的一个BUG,在芯片数据手册中历史版本的更改记录中可以看出增加了第5页中的Changed VCC = 0 to VCC needs a pulse。