This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165 CTRL 引脚控制问题

我是按数据手册推荐搭建的电路,我在调试电路时出现问题,现请教各路大神。

当VIN=3.3V,输出串联4个LED时,CTRL能有效控制灯的亮灭,当CTRL=VIN,灯亮,接地灯灭,电路工作正常,

但是当输出串联8个LED时,CTRL端高电平,灯亮,但是把CTRL置地时,灯还一直亮着,LED一直亮,CTRL无法控制灯的亮灭,但是当把VIN=10时,CTRL又能有效控制灯的亮灭了?实在想不明白为什么这样?

PS:LED的驱动电流是40mA,正向导通压降3V。