想使用tps61196做一款背光调节芯片,但spec写此稳压器 提供 50mA 至 400mA 范围内可调的 LED 电流 ILED=1.229*3992/R ,有时候背光电流小于50mA;如何实现ISET电阻的设置能让这款芯片输出范围在1mA~200mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想使用tps61196做一款背光调节芯片,但spec写此稳压器 提供 50mA 至 400mA 范围内可调的 LED 电流 ILED=1.229*3992/R ,有时候背光电流小于50mA;如何实现ISET电阻的设置能让这款芯片输出范围在1mA~200mA
你好,这款器件可以多串LEDK并联使用吗?比如四串灯的A 连接在一起,K连接在一起,需要总共240mA,可否设置ISET电阻为60mA,让IFB1,2,3,4并联输出满足需求吗?