This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92691输出存在跌落,并且缓启动以及斜坡补偿感觉不正常

原理图如下,输入是18-24V,输出为41V,电流约为0.5A

测试电路的VIN 以及 GATE引脚波形如下:

然后根据公式计算comp的阻容值,然后更换之后波形如下

然后将COMP管脚连接一个1MΩ电阻到地,并且去掉两个4.7uF电容,波形如下:

现在我也不知道这么配置是不是正确,因为根据datasheet计算出来的值测试的波形存在问题,而且斜坡补偿和缓启动这块的原理我有点不太理解,各位大神能不能帮忙解答一下,谢谢!