LM5175和LM5176是PIN to PIN 兼容的,这两款产品在性能参数和稳定性上有什么区别吗?从规格书上看不出多大的差别
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Parametrics |
LM5175 |
|
Topology |
Buck/Boost |
Buck/Boost |
Vin(Max)(V) |
42 |
55 |
Vin(Min)(V) |
3.5 |
4 |
Iq(Typ)(mA) |
1.65 |
2 |
Features |
Adjustable Current Limit,Enable,Frequency Synchronization,Power Good,Pre-Bias Start-Up,Synchronous Rectification,UVLO Adjustable |
Adjustable Current Limit,Enable,Frequency Synchronization,Power Good,Pre-Bias Start-Up,Synchronous Rectification,UVLO Adjustable |
Hi
前者可利用脉冲跳跃来选择连续导通模式 (CCM) 或断续导通模式 (DCM),后者是强制连续导通模式 (FCCM)
其次就是输入电压范围不同。
我现在采用LM5175做的电源,主要工作在Buck模式,8~24V转4.5V。
有这样一个问题:电源正常工作一段时间后,可能是几分钟或几小时。SW2波形就不正常了,且不再恢复正常。正常SW2大约每1ms下拉一次,给Cboot2充电。不正常时,SW2每个周期都会下拉一次,示波器看见Cboot2电容电压下降很快,需要每个周期补充能量。
断电万用表测得SW2和Boot2之间电阻只有100多欧姆。取掉Cboot、充电Diode,测得的阻值仍为100多欧姆,应该是LM5175本身损坏。这种情况下,输出正常。SW1波形正常,但LM5175很烫。