This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01622: 在USB Type-C电源传输以及AC/DC适配器方案中,使用UCC28780的优点有哪些?

Other Parts Discussed in Thread: UCC28780

在高效率和高功率密度的USB Type-C电源传输以及AC/DC适配器方案中,使用UCC28780的优点有哪些?

TIDA-01622是一款经过全面测试的TI参考设计,适用于高效率和高功率密度的USB Type-C电源传输以及AC/DC适配器方案, 可广泛应用于需要宽输入电压范围(85 - 265VAC)的笔记本电脑适配器和智能手机充电器等应用场景。

UCC28780作为关键的PWM控制器,对于实现94%的峰值效率和30W/in3的高功率密度,其自适应零电压开关(ZVS)和突发控制的特点起到了重大作用,同时也容易满足严格的全球效率标准DoE Level VI和EU CoC V5 Tier-2。

关于这个主题更多的信息, 请参考User Guide for TIDA-01622的第2.3章节 " System Design Theory " 。你也可以从TIDA-01622 folder,下载更多的参考设计文件 (BOM, 原理图, Gerber) 。