请问下我用了BQ25606做电源管理,规格书上写的SYS电压最低到3.5V,不会再降低了,可是我再实际电路板上测量SYS引脚输出电压会比3.5V还低,不充电状态,SYS始终和电池电压差零点几伏,请问下这是什么情况?这个现象正常么?有没有什么方法可以把 SYS引脚的最低电压阈值卡在3.5V以上?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,目前VSYS后端是一个按键开关,关闭开关后只有充电IC部分电路工作,这时候VSYS电压输出为4.06V;
目前输入端使用的是5V-2.4A的USB充电器,另外上午的时候也试过另外两款手机的充电器,规格是5V-2A,充电电流仍然是1A。
另外该测试中,我将万用表串接在5V的 VBUS输入端,可能会受万用表内阻影响,但是我尝试了修改Richg电阻阻值到330R,Rilim阻值到100R,在同样环境下测试,充电电流仍然是1A
测量方式不太正确。充电芯片的输出到电池的线尽可能用最短的粗线来连接。你这样的接法会导致线路上的阻抗很高,在大电流的情况下,线上压降比较高。
你可以用万用表直接测充电芯片输出端的电压是多少?芯片有可能以为电压电压已经到4.2V了。
你好,根据之前的提示,我好像已经找到了问题所在了,该项目USB接口部分除了用作充电之外,还兼容了程序烧写功能,D+/D-网络另外有接到一颗USB转串口的IC,插USB充电的时候,测量了D+电压为3.2V,D-电压为0V;
我将USB转串口IC去掉后,充电电流可以达到1.5A以上,VSYS可以达到4.2V。
请问下:D+=3.2V,
D-=0V
会把充电电流限制在1A 么?