This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61030在轻负载下会有很高的Burst电流

Other Parts Discussed in Thread: TPS61030

我在测试系统耗电的时候发现TPS61030在轻负载下会有很高的Burst电流,应该和TPS61030进入了Power Save mode有关。请帮忙和原厂确认一下这个瞬间电流的大小是否正常?同时这个电流引起了整个系统耗电的RMS值很高,是否会对系统耗电带来较大影响?谢谢!

 

     下图是从TPS61030输入端(3V电源输入)测到的耗电情况,可以看到DC值只有1.75mA,而RMS值已经到了20mA,瞬间电流达到了270mA。

 

     下图是断开TPS61030的输出端,直接用电源(5V)供电给后端测量到的实际耗电情况,可以看到后端系统耗电的DC值只有0.9mA,RMS值也只有1.1mA,瞬间电流为7.8mA,符合蓝牙芯片的待机耗电状态。

 

我们板子上的电路图如下: