This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TPS5430外部RC补偿电路问题

Other Parts Discussed in Thread: TPS5430

TI工程师您好!

问题一:

最近使用贵司TPS5430芯片,24V转15V,看datasheet page15-16以及figure14写道,用陶瓷电容的话需要附加的RC电路来稳定电路(即Figure14中的R3 C4 C6 C7)。我想问,附加的RC网络是强制还是推荐?若不加,会出现什么异常现象?为什么陶瓷电容会使得电路不稳定?是因为陶瓷的ESR小吗?看文档slv237c中写道,似乎只有有限的几种电容搭配TPS5430的时候(如POSCAP),电路不用附加RC来调整电路的零点和极点。是这样么?

我的电路按照最简设计,Vin=24V,Vout=15V,电容电感的均设计较大,Cin=10uF(钽电容),Cout=220uF(铝电解电容),Lout=47uH,没有附加的RC补偿网络,是否可行?如下图

问题二:参考文档slva257a,用TPS5430产生负压(24V变-15V),RC补偿电路的器件值计算方法与24V变+15V中的计算方法一样吗?能否给出参考设计?

急待回复,非常感谢~!