使用TPS74401
输入:5V
输出3.3V
电流:1A
环境温度:70
我们通过热仿真得出,芯片的结温是99摄氏度左右,芯片顶部有导热垫。芯片手册上写的结温范围是-40~+125
不知道这个设计是否有问题?需要在这个环境温度下工作10小时左右。
感谢大家啦!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS74401
输入:5V
输出3.3V
电流:1A
环境温度:70
我们通过热仿真得出,芯片的结温是99摄氏度左右,芯片顶部有导热垫。芯片手册上写的结温范围是-40~+125
不知道这个设计是否有问题?需要在这个环境温度下工作10小时左右。
感谢大家啦!!!
你好,
输入5v,输出3.3v,压降为1.7v.
负载电流为1A。
功耗为1.7W
算一下芯片的温升=热阻*功耗=JA*1.7=...
你环境温度是70,可以接受的温度是125来算的话,温升55.
你可以算一下可以工作吗.
谢谢。