使用TLV62130 输出3.3V 3A 给FPGA 3.3V bank供电,实测发现输出电压4.0V ,FPGA加载程序后上升到4.3V,下图电路在其他电路板上已经验证过可以正常使用,测试en信号均正常,检查FPGA器件正常。目前在查询2.2uH电感是否能达到5A电流值。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TLV62130 输出3.3V 3A 给FPGA 3.3V bank供电,实测发现输出电压4.0V ,FPGA加载程序后上升到4.3V,下图电路在其他电路板上已经验证过可以正常使用,测试en信号均正常,检查FPGA器件正常。目前在查询2.2uH电感是否能达到5A电流值。
谢谢各位的建议,已经查到问题了。确实是被fgpa拉高的,断开负载后电源正常工作。