This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5035的外同步频率功能问题

Other Parts Discussed in Thread: LM5035

各位前辈:

最近在调试LM5035的外同布频率功能。

按照手册推荐,我在RT引脚外串联了100pF电容,然后注入270kHz~330kHz,幅值0-3.3V,占空比 0.5的PWM波。手册上说,RT引脚正常的偏置电压是2V,注入的同步频率高电平要大于3.2V。可是这样的PWM注入后,电源不稳定,输出纹波会自激到200mV,正常纹波是50mV,频率300kHz。后来,我把幅值调到-0.3V~2.6V,发现电源可以被同步,而且稳定。

现在就有疑惑了。手册推荐外同步频率要高于电源频率10%,也就是330kHz,可是注入的频率在270kHz~330kHz也可以,这是为什么?

手册推荐要高电平大于3.2V,而我注入3.3V会自激,注入2.6V却正常,这又是为什么呢?