This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP road map

Other Parts Discussed in Thread: DLP3010, DLP4500

你好,我们目前遇到DLP芯片选型的问题。请问DLP的roadmap,也就是每种型号的停产和在产信息在哪里看。

  • 您好!

    感谢您使用TI的DLP产品。

    您可以直接在TI.com找到对应的芯片,然后在order now界面中查看。

    请选择ACTIVE的产品。

    希望这个回答可以帮助到您。

  • 你好,谢谢回复,还有两个问题:
    1、我看到DLP3000的状态是lifebuy ,是以后有停产的计划吗?
    2、替代产品是DLP3010,该芯片的翻转方式与DLP3000是不同的,我们的光路需要DLP3000的翻转方式,请问DLP3010的像素翻转方式能否控制,使得翻转方式与DLP3000是相同的,角度为12°。
    祝好!
  • 您好:
    1.各种状态的解释如下
    ACTIVE: Product device recommended for new designs.
    LIFEBUY: TI has announced that the device will be discontinued, and a lifetime-buy period is in effect.
    NRND: Not recommended for new designs. Device is in production to support existing customers, but TI does not recommend using this part in a new design.
    PREVIEW: Device has been announced but is not in production. Samples may or may not be available.
    OBSOLETE: TI has discontinued the production of the device.
    2.DLP3000是菱形像素DLP3010是manhattan像素,DLP3010没有办法像DLP3000那样翻转,DLP4500和DLP3000具有相同的菱形像素。