您好,大概一年前我在TI公司购买了一个DLP LightCrafter 4500模块,当时为了使用方便曾经将DMD和电路板拆下,不过最近发现DMD上的镜子无法控制,无论从GUI导入什么图案,DMD镜子的状态都无法改变,显示乱码的状态,不知道什么原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,大概一年前我在TI公司购买了一个DLP LightCrafter 4500模块,当时为了使用方便曾经将DMD和电路板拆下,不过最近发现DMD上的镜子无法控制,无论从GUI导入什么图案,DMD镜子的状态都无法改变,显示乱码的状态,不知道什么原因。
您好!
DLPC350初始化时可以完成的,问题可能在DMD端,使用内部的测试pattern是否也是一样的问题?能否提供问题的照片
1.建议检查DMD和PCB板的接触是否良好,软排线的连接、通路是否良好
2.建议检查DMD端的供电是否正常
3.是否有可以更换的DMD,可以尝试更换DMD
谢谢