This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC910和DLP9000能否组合应用

Other Parts Discussed in Thread: DLPC910, DLPC900, DLP9000X, DLP9000

在DLPC910的手册上还是DLP9000的手册上,都是两个DLPC900+DLP9000或者DLPC910+DLP9000X,或者DLPC910+DLP600,始终没有看到关于DLPC910和DLP9000组合应用的描述,请问是什么原因?

  • 您好!

    感谢您关注TI的DLP产品。

    DLPC910和DLP9000不能组合使用,TI的每一款DLP都有其对应的控制器。

    DLP9000X是比DLP9000更高速度等级的DMD。DLPC900是基于ASIC的控制器,其支持的最高输出频率是400MHz,而DLPC910是基于FPGA的控制器,其支持的最高输出频率是480MHz。

    另外,DLPC900内部会视频处理的功能,而DLPC910内部没有视频处理功能,需要外部额外的微控制器系统来帮助完成。

    所以两者之间存在较大的差异。

    希望这个回答可以帮助到您。