This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PAD1000的应用性技术问题

Other Parts Discussed in Thread: DLPC2607, DLP2000

1.一般条件下,PAD1000的正常工作时,芯片体表温度是多少?

2.一般条件下,PAD1000芯片会因为高温而停止部分功能吗,如果是,那大概温度是多少?

3.同等电路条件下,一块工作时温度达70摄氏度,另一块40摄氏度,产生这两种情况是什么原因(电路正常,无短路,无虚焊)?

4.PAD1000在贴片时,对贴片的工艺有何要求?

  • 您好!

    感谢使用TI的DLP产品。

    1)芯片表面温度与很多因素有关,环境温度,芯片工作状态等等,只要在芯片允许的温度范围内都是可以的。

    2)只要在芯片推荐的温度范围内,芯片都是会正常工作的,请参考芯片数据手册:

    3)您可以尝试做交叉实验进行对比,也可以检查下该芯片的外围电路是否有区别,如果在相同的工作条件下通常不会出现这么大的温差

    4)没有特殊的要求

  • 如果因为散热不好的原因,导致这颗芯片所在的环境温度超过了85度,但是芯片本身的温度没有达到125度的情况下,有没有可能造成芯片不工作的可能
  • 我们目前遇到的问题是光机正常工作的情况下,几个小时后会自动熄灭。是PAD1000自动跳为低电频。请问为什么呢?
  • 您好!

    芯片内部是有热保护电路的,如果温度过高会自动shutdown,请参考数据手册

      如果是怀疑过热造成的问题,可以增加散热片或者风扇再做测试。

    请问具体的使用环境是怎么样的,是与DLP2000和DLPC2607搭配使用吗?