菜鸟新入手TMDXLCDKC6748板子,想将其计算能力与F28m35比较一下
1、F28m35是186MMIPS,C6748是3600MMIPS,同一段程序是不是C6748的执行时间比F28m35快20倍
2、怎样才能使C6748的计算达到最高速度,哪位朋友有相关的demo能够参考一下
3、C6748的程序怎么固化
非常感谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
菜鸟新入手TMDXLCDKC6748板子,想将其计算能力与F28m35比较一下
1、F28m35是186MMIPS,C6748是3600MMIPS,同一段程序是不是C6748的执行时间比F28m35快20倍
2、怎样才能使C6748的计算达到最高速度,哪位朋友有相关的demo能够参考一下
3、C6748的程序怎么固化
非常感谢!!!
小菜非常感谢Titan的解答
还有一些疑问,我把程序放在在L2RAM中,然后将优化级别调到了-o3,参考了一下cache_mme例程里面的关于cache的配置,是不是直接调用CacheEnable(L1PCFG_L1PMODE_32K | L1DCFG_L1DMODE_32K | L2CFG_L2MODE_256K);就可以了啊,最后我测试了一下,发现计算速度没有改观(连仿真器的条件下)
这样会不会使得整个L2RAM变成了cache,无法当做SRAM使用啊
还想麻烦Titan能够教我一个详细的发挥c6748最大运算性能的步骤和方法
多谢!!!