硬件环境:研旭28335开发板、XDS100V2仿真器
软件环境:CCS6.0
目前遇到的问题:
1、连接仿真器时:RUN-conncet target之后显示连接成功
过大概10s后,显示如下报错信息
C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.450.0)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
然后显示连接失败
请问这是什么原因?
ps:在10s内,趁其不注意可以快速run-load-load programme,然后马上run-resume可以实现仿真
但仿真时间持续大概几秒,会显示disconnected running
跑马灯虽然还在跑,但此时连接已经失效了
若此时再重新连接TARGET,会显示151错误
C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.1.450.0)
目前经过搜索可能是以下原因:
1、FLASH锁死
2、仿真器驱动问题
3、ccs6.0问题
求助各位大大~