This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

一个关于28075中ADC的问题

   请问一下,为什么当我从外部给一个AD引脚加上电压,该AD引脚相邻的下一个AD引脚上也会测出有电压呢?

   举个例子,我仅在ADCINA2引脚上加上2.5VDC(或1.2VDC),测得在ADCINA2引脚上的电压的确为2.5VDC(或1.2VDC),没有问题。但是同时测得ADCINA3引脚上有一个0.35VDC(或0.16VDC)左右的电压,其余的 ADC引脚上电压则均为0正常。同理在ADCINA3引脚加上电压时,也会在ADCINA4引脚上检测出来较小的电压......

   实在不知道是怎么回事,希望能够解答一下,有没有什么可能的原因导致了这个问题。