This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640工作电压纹波的问题

Other Parts Discussed in Thread: CC2640

使用CC2640的板子,有一定比例会不工作,(大概5%左右),不工作的板子有两种现象:1、晶振不启振(确定不是晶振问题),2、晶振启振但程序不运行。

故障是在单板测试、组装测试和使用中都会出现,所以应该是设计的问题。

我的板子上是有升压boost的,这个芯片造成给CC2640的供电电压出现比较大的纹波,大概幅度有60mV-80mV,VDDR的纹波大概也有20mV左右。

另外,CC2640有个这个要求:

请问,是不是因为这个原因,造成CC2640工作不正常?

  • A certain proportion of the plates using CC2640 will not work (about 5%), and there are two phenomena in the plates that do not work: 1. Crystal vibration will not start (it is determined that it is not a crystal vibration problem); 2.Crystal oscillator starts but the program does not run.

    Failures occur during veneer testing, assembly testing, and use, so they should be design issues.

    There is a boost on my board. This chip causes a relatively large ripple in the power supply voltage to CC2640, which is about 60mv-80mv, and about 20mV ripple in VDDR.

    In addition, CC2640 has this requirement:

    Is it because of this reason that CC2640 is not working normally?

  • 这边是E2E china论坛,直接用中文就行。涉及供电了我不专业,帮你@AZ
  • Bing,

    应该不是Slew rate的问题,这个是整个电压上下点的速率。

    我看你好象是交流偶合看纹波,绝对电压值是多少呢?

    你可以看一下上下电的时序,看看reset/vcc/vddr等电压。

    另外,你是怎么判断一定不是crystal的问题呢?你可以把规格书po上来我看看,或者你用TI推荐的crystal 验证一下。swra495f_Crystal Oscillator and Crystal Selection.pdf

    BR. AZ

  • 我之前发了中文的,没人理我,所以发的英文。
  • 感谢您的回复,回答您的质疑:

    1、直流电压是2.8V左右,我用通信电源和电池都试过,结果都是一样的,所以跟直流电压没有关系。

    2、不知道您说的上电时序指的是哪方面,但是我把VCC、VDDR、reset的上电图发出来看看。

    VCC上电图

    VDDR上电图

    reset上电图

    帮看看有啥问题。

    3、判断不是晶振问题原因是,曾经把不启振板子上的晶振换到正常板子上,可以启振的。也将不起振的板子上的CPU换新的,重新烧录后可以正常工作。不过我现在的晶振两脚之间没有加1M的电阻,不知道是不是影响很大。下面把晶振规格书发上去,帮忙参考一下。

    GSC03T-210009-24.00MHZ贴片无源晶体振荡器.pdf

  • bing, 

    晶振从规格书上看,是没有问题的。1Mohm或许有帮助,但不是必须的。

    三个时序也没问题。这个是有问题还是没有问题的时序呢?

    我看你的纹波有60mV?那么,2.8V-60 mV应该也是在工作范围之内的。

    你把原理图po上来我看看吧。

    BR. AZ

  • 您好,回答您的疑问:

    1、这个时序都是不起振的板子的,是同一块板上的时序。

    2、纹波是有60mV-80mV的,不过加大电源电容可以减小,我加了两个大概37uF的电容,可以减小到20mV多。

    3、原理图我用pdf文档上传。TEETHB-V1.2.pdf

  • C8/C9 27pF?

    射频指标测试过了吗?

    BR. AZ

  • 1、的确是27pF,30多pF的也试过,一样不启振。
    2、射频只测了场强大小,其他没测。本来是有使用巴伦的,后来想用电容和电感来代替,最后发现直接接,场强信号也够(距离30cm的位置,实测场强信号有-55~-62dbm),所以就没用巴伦。这个会跟CPU损坏有关?
  • B ing, 

    27太大了,你需要测试一下频偏。

    如果按照TI的参考设计来说,(9pF的负载电容),外置CL是不用焊接的。

    BR. AZ