This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1310射频功耗

Other Parts Discussed in Thread: CC1310

cc1310每秒唤醒2次射频的瞬间电流是6ma

  • 你的问题是什么?
  • 以下是CC1310的电流参数,射频时的电流是比较高的:
    RX:5.4mA
    TX(+10dBm 时):13.4mA
    Coremark 运行时的 48MHz 有源模式微控制器 (MCU):2.5mA (51µA/MHz)
    有源模式 MCU:48.5 CoreMark/mA
    有源模式传感器控制器(24 MHz):
    0.4mA + 8.2µA/MHz
    传感器控制器,每秒唤醒一次来执行一次 12 位 ADC 采样:0.95µA
    待机电流:0.7µA(实时时钟 (RTC) 运行,RAM 和 CPU 保持)
    关断电流:185nA(发生外部事件时唤醒)