请问CC1352P1 是否能通过ti15.4-stack的collector和sensor范例中使用多个collector设备组成一个大型的星型网络?如果可以那collector和sensor是通过相同的pan id进行匹配的,那不同的sensor移动到不同的collector网络时如何切换?如果过不行用哪个方案比较合适?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The CC1352R device is a multiprotocol Sub-1 and 2.4-GHz wireless MCU targeting Wireless M-Bus, IEEE 802.15.4g, IPv6-enabled smart objects (6LoWPAN), Thread, Zigbee®, KNX RF, Wi-SUN®, Bluetooth® 5 Low Energy, and proprietary systems.
CC1352R支持蓝牙,CC1352P内置PA。
至于你说的信号值为RSSI:
static void dataIndCB(ApiMac_mcpsDataInd_t *pDataInd)
ApiMac_mcpsDataInd_t 里面包含的RSSI的值。
也就是:
case MAC_MCPS_DATA_CNF:
if(pMacCallbacks->pDataCnfCb)
{
/* Confirmation structure */
ApiMac_mcpsDataCnf_t cnf;
/* Initialize the structure */
memset(&cnf, 0, sizeof(ApiMac_mcpsDataCnf_t));
/* copy the message to the confirmation structure */
cnf.status = (ApiMac_status_t)pMsg->dataCnf.hdr.status;
cnf.msduHandle = pMsg->dataCnf.msduHandle;
cnf.timestamp = pMsg->dataCnf.timestamp;
cnf.timestamp2 = pMsg->dataCnf.timestamp2;
cnf.retries = pMsg->dataCnf.retries;
cnf.mpduLinkQuality = pMsg->dataCnf.mpduLinkQuality;
cnf.correlation = pMsg->dataCnf.correlation;
cnf.rssi = pMsg->dataCnf.rssi;
cnf.frameCntr = pMsg->dataCnf.frameCntr;
之前看好像说1352R中蓝牙2.4G和433的只能用其中一个不能同时使用,是这样吗?而1352P就可以两个同时使用是吗?
ti15.4-stack多collector多sensor的时候因为涉及到下发消息到其中某一个sensor的,那时候是通过什么确定是哪个sensor?能用mac地址吗?
因为刚开始学ti,请问哪里有入门相关的资料?例如开始第一个工程和开发工具使用之类的!