3.0.1版本的协议栈多了许多老协议栈没有的特性,手里有基于3.0.1版本的CC2530的Coordinator和基于2.5.1a的一个CC2530Router,请教一下,在不改变Router的协议栈版本的情况下如何改动Router,使得2.5.1a的设备可以被3.0的设备接纳入网?因为有许多基于2.5.1a的终端设备,不方便做改动,谢谢大家!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for your answer.
There still exsit a problem that right association request and response could be made between Coordinator and Router:after the association procedure,the Coordinator of 3.0 succeed to send an APS Transport Key Command to Router of 2.5.1a,then Router made the Acknowledgement.The Router should send a Device Annouce to Coordinator to join successful but it did't make it.
It seems like Coordinator recognized Router,but Router did'nt want to join.What should I do to make Router send Device annouce command? Thanks a lot.
Device used SampleLight project of 2.5.1a to join a network of 3.0.1,the sniffer file was caught by ubiqua.I think the Router failed to run his security moudle so that it can not decrypt the APS command?2.5.1a join 3.0.1.rar
Hello , i meet the same problem , have you solved it yet ?wish your reply thanks