Packet Error Rate Example Application
The Packet Error Rate (PER) example showcases different RF transfer modes of the CC13xx. It combines tasks, events and several peripherals to a platform- independent application and runs on all CC13xx launchpads as well as the CC1310EM/SmartRF06.
Test cases are provided for the following RF modes:
Custom
: Custom settings to be exported from SmartRF Studio to the smartrf_settings.c file2-GFSK
: Generic frequency shift keying with binary symbols, 50 kBit/sLR Mode
: Legacy Long Range (625 bps)OOK
: On-off keyingHS Mode
: High-speed mode with up to 4 MBit/sSL LR
: SimpleLink Long Rang (5 kbps)BLE
: Bluetooth Low Energy (CC135X only)
Note that when running the CC1310-CC1190, CC1350 (433 MHz) or CC1352 Launchpads, HSM and OOK are not supported by the PER test. Additionally, the Legacy Long Range Mode (LRM) is not supported on CC1352.
Peripherals Exercised
This example uses the following CC13xx peripherals:
- RF core for radio communication
- 2 GPIOs for buttons
- 3 GPIOs for controlling the CC1190 when running CC1310-CC1190 Launchpad
- SPI to drive the LCD displays on the boards
- UART0 (115200 Baud) as an alternative display on VT100-compatible terminal emulators
Peripheral | Identifier | CC13xxEM/SmartRF06 | CC13xx Launchpad | CC1310-CC1390 Launchpad |
---|---|---|---|---|
Select button | Board_PIN_BUTTON0 | UP | BTN-1 | BTN-1 |
Navigate button | Board_PIN_BUTTON1 | DOWN | BTN-2 | BTN-2 |
Display | – | LCD Dogm1286 | Display Booster Pack | Display Booster Pack |
CC1190 Control | Board_HGM | – | – | DIO28 |
signals | Board_LNA_EN | – | – | DIO29 |
Board_PA_EN | – | – | DIO30 |
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
This example requires two boards, each running the PER Test application. However, the packet format is identical to the default one in SmartRF Studio, so that any compatible hardware can be used as well.
Connect a display to the board or alternatively, use the UART and hook it to a VT100-compatible terminal emulator at 115200 Baud. Use PuTTY or TeraTerm on Microsoft Windows. On Linux, use the terminal emulator that is shipped with your distribution. After a splash screen, you will see the main menu (the range extender option (CC1190) is only shown for CC1310 LAUNCHLX):
Main Menu >Test: 2-GFSK Freq: 868.0 Pkts: 10 CC1190: Disable Mode: Rx Start...
Navigate through the rows with BTN-2/DOWN, modify a value or start the selected test with BTN-1/UP. Note that it is the user’s responsibility to enable CC1190 from the menu when running CC1310-CC1190 LAUNCHXL.
Use a second board with the PER test application as test companion for transmissions. Once started, the current progress is shown with these menus (TX mode on the left side, RX on the right):
Sending... | Receiving... 2-GFSK 868.0 | HS Mode 868.0 | Pkts ok : 39 Pkts sent: 47 | RSSI [dBm]: -74 | PER [%] : 17.01 | | Push a button | to abort.
The receiver prints the amount of successfully received packets (Pkts ok), the Signal strength of the current packet (RSSI) and the observed packet error rate (PER) in percent. Please note that the PER is n/a when sending more packets than configured in the receiver.
- You can always abort a running test case by pushing any button and go back to the main menu.
Application Design Details
The PER test application contains of one main task and an event handler to synchronize the task with buttons. After setting up all resources, the menu task is started and runs in an endless loop. It shows the menu and invokes test cases in either rx.c
or tx.c
.
Changelog
Version 1.1
- released with TI-RTOS 2.17
- add version number on the splash screen
- hide cursor on VT100 terminals
Version 1.0
- shipped along with the CC1310 launchpads as default application
Version 2.0
- released with TI-RTOS 2.21
- added support for CC2650_LAUNCHXL and CC2650DK_7ID
- added BLE mode for CC1350 and CC2650 platforms. Note that the default frequency is 2.402MHz, which is an advertisement channel and may result in packet errors due to BLE devices advertising.
- added custom mode which takes settings exported from SmartRf Studio into rfPacketErrorRate_<platform>\smartrf_settings
Version 2.1
- released with simplelink_cc13x0_sdk_1_10
- added support for SimpleLink Long Range (5 kbps)
- added support for CC1310-CC1190 LAUNCHXL. When running on this HW, it is the user’s responsibility to enable CC1190 from the menu. Note that HSM and OOK is not supported in the PER test when running on this HW
Version 2.2
- released with simplelink_cc13x0_sdk_1_50_00_00
- added support for CC1352 and CC1350 (433MHz) LAUNCHXL. These boards support a reduced set of modes
- added a No-RTOS version of the code