Version 1.0.1 ============= Overview ======== This is the mmWave SDK out-of-box demo lab for the TI IWR68xx EVM. The mmWave Demo stores chirp configuration information on the device and does not require external input to start the sensor. This allows the device to be used with custom GUIs and visualizers. The demo source code is pulled from the mmWave SDK when the project is imported into CCS. Features ======== The following features are supported: * Supports IWR6843 ES2.0 devices. * Supports mmWave SDK 3.5.x.x New and Updated Features ======================== The following is a list of new and updated features for this release: * N/A Resolved Incident Reports ========================= Table 1 provides information on Incident Report (IR) resolutions incorporated into this release. **Table 1**: Resolved IRs for this Release IR Parent/Child Number | Severity level | IR Description -----------------------|----------------|---------------- N/A | NA | See mmWave SDK Release Notes Known Issues ============ Table 2 provides information on IRs that are known issues for this release. **Table 2**: Known Issue IRs for this release IR Parent/Child Number | Severity level | IR Description -----------------------|----------------|---------------- N/A | NA | See mmWave SDK Release Notes Work Arounds for Major Known Issues =================================== The following are workarounds for each known issue with a major severity that exists in this release: * N/A Limitations ========================= The following is a list of known limitations for this release that were known at the time of release: * N/A