TMS320C6748 GEL, CCS Setup, & BSL Files              1014014A_Release_Notes.txt
-------------------------------------------------------------------------------

Version:   1.0
Hardware:  TMS320C6748
Date:      8/26/2009

-------------------------------------------------------------------------------

This ZIP file contains the GEL, CCS setup, and BSL files for the TMS320C6748
SOM-M1. These files are also available on the Code Composer Studio v3.3 IDE CD.

---------------------------
Table of Contents
---------------------------
1 Installation Instructions
2 History
3 Known Issues
---------------------------

-------------------------------------------------------------------------------
1) Installation Instructions
----------------------------

The installation process involves copying the contents of this ZIP file to 
different locations on a development PC where Code Composer Studio (CCS) has 
already been installed. The locations given below point to the same directories
where the CD install shield places the files; however, you may place them in a 
different location of your choosing.

--) Copy the entire "evmc6748_v1" folder here: 
    C:\CCStudio_v3.3\boards\

--) Place a copy of the GEL files here:
    C:\CCStudio_v3.3\cc\gel\

--) Place a copy of the CCS setup files (in the "import" folder) here:
    C:\CCStudio_v3.3\drivers\import\

-------------------------------------------------------------------------------
2) History
----------

--) Initial v1.0 release

-------------------------------------------------------------------------------
3) Known Issues
---------------

--) None

-------------------------------------------------------------------------------
Copyright (c) 2009 Logic Product Development Company            www.logicpd.com