Creating a Bootable Demo
------------------------
This file contains instructions for creating and flashing a bootable demo into the SPI Flash that will run when the eZDSP is powered.

There are three major steps in flashing the demo.
1. Creating the demo program.
2. Creating the boot image.
3. Programming the boot image.

Creating the demo program
-------------------------
    This is a program that runs when the eZDSP is powered. Create a project with all the necessary setup and build it  to get a .out file. The "boot_post" test can be used for this.
Creating the boot image
-----------------------
The demo program needs to be converted to a bootable format for the boot image. This can be done by the following steps.
1. Copy the Demo program (.out file) to the folder "ezdsp5535_v1\boot_post\hex_utility".
2. In that directory, edit the last line and second last line of "demo.cmd" to reflect the input (.out) and output (.bin) file respectively.
3. Go to the Windows command prompt and change directory to the "hex_utility" directory.
4. Enter the following command in the command prompt:
   hex55 demo.cmd
5. The output .bin file will be created in the same directory.

Programming the boot image
--------------------------
This involves flashing the .bin boot image to the SPI Flash. 

WARNING!
The SPI boot takes precedence over the SD card boot. So the SPI Flash must be erased or disabled to boot from the SD card after this.

Follow the steps below to program the demo on the SPI Flash.
1. Open Code Composer Studio configured for the eZDSP. Use the gel file provided with the target content (ezdsp5535_v1\gel\ezdsp5535.gel).
2. Load and run the "spiflash_writer" program which can be found in "ezdsp5535_v1\boot_post\spiflash_writer".
3. The program will ask for a file name. Enter the full path of the .bin file created earlier.
4. The program will write the file to flash and verfy it. Wait for the "All Tests Passed" message.
5. Verify the demo by disconnecting from Code Composer and power cycling the board (Remove USB connector J2 then plug it back in).
6. The reset due to power cycling will cause the boot loader to load the program from the SPI Flash and run it.