1. Unzip this example directory to a desired location.

2. Boot EVM in No Boot mode.

3. Launch CCS and connect to GEM core 0. Follow instructions in MCSDK norwriter README (C6657). Change "app.bin" in norwriter_input_txt to "app.dat"

4. Load spirom_le_swap.dat into address 0x80000000 and copy the .dat file into the bin directory of the norwriter. Load norwriter .out file and run.

5. Reboot EVM into NAND mode. To do this, configure dip switches:

SW3 {pin 0 - pin8) = 10110000 (0-ON, 1-OFF)

SW5(pin0 -  pin8) = 00100000

DDR should be configured by the boot image. To test, connect to GEM core 0 and navigate to address 0x80000000 in the memory browser in CCS.