# Generated by Code Composer Studio

# Makefile for C:\CCStudio_v3.1\boards\DSK5509A_V1\examples\dsk_app_idle\dsk_app_idle.pjt
# This makefile is intended to be compatible with any version of make.
#
# USAGE
# Step 1: Set up proper environment variables, by running DosRun.bat
#         (Windows platform) or set them up by yourself.
# Step 2: Change directory to the directory of this makefile, which is stored
#         in the macro MAKEFILE_DIR
# Step 3: In the makefile directory, you can perform one of these operations:
#         To build the configuration <config>, type make <config>
#         To clean the configuration <config>, type make <config>clean
#         To rebuild the configuration <config>, type make <config>rebuild
#         If <config> is not specified, the operations apply to the active
#         configuration, which is stored in the macro ACTIVE_CONFIG.
# For CCS gmake users: In the makefile directory, you can perform one of these operations:
#         To build the configuration <config>, type gmake projectName.mak <config>
#         To clean the configuration <config>, type gmake <config>clean
#         To rebuild the configuration <config>, type gmake <config>rebuild
#         If <config> is not specified, the operations apply to the active
#         configuration, which is stored in the macro ACTIVE_CONFIG.
#
# DETAILS
# Step 1:
#   In order for this makefile to work, you must have the environment variables
# set properly.  Specifically, the paths to build programs and the system-wide
# header files and library files must be set.
#   In Windows, a batch file "DosRun.bat", located at the root directory of
# the Code Composer Studio installation, is provided to set up these variables.
#   In UNIX, you can set up these environment variables yourself.  The "PATH"
# variable must include the paths to the build programs, and the "C_DIR" and
# "A_DIR" variables must include the paths to the system-wide header files and
# library files.
#
# Step 2:
#   System files referenced by this project are specified in full path names,
# while other files in this project are specified in path names relative to the
# directory of this makefile.  These directory names are stored in DIR_x macros.
# You can modify them to reflect the locations of the files on this system.
#   It is important that the command to make this makefile is issued from the
# directory of this makefile, which is stored in the macro MAKEFILE_DIR.
#
# Step 3:
#   There are three operations that can be performed on a build configuration:
# make, clean, and rebuild. A rebuild forces all files in the configuration to
# be rebuilt.
# To build the configuration <config>, type make <config>
# To clean the configuration <config>, type make <config>clean
# To rebuild the configuration <config>, type make <config>rebuild
#   If <config> is not specified, the operations apply to the active
# configuration. The active configuration can be any valid build configuration
# (including "all") and is specified in the macro ACTIVE_CONFIG.
# To build the active configuration, type make
# To clean the active configuration, type make clean
# To rebuild the active configuration, type make rebuild
#
# For CCS gmake users:
#   There are three operations that can be performed on a build configuration:
# make, clean, and rebuild. A rebuild forces all files in the configuration to
# be rebuilt.
# To build the configuration <config>, type gmake projectName.mak <config>
# To clean the configuration <config>, type gmake <config>clean
# To rebuild the configuration <config>, type gmake <config>rebuild
#   If <config> is not specified, the operations apply to the active
# configuration. The active configuration can be any valid build configuration
# (including "all") and is specified in the macro ACTIVE_CONFIG.
# To build the active configuration, type gmake
# To clean the active configuration, type gmake clean
# To rebuild the active configuration, type gmake rebuild

# The MKFLAGS macro takes the place of the MFLAGS or MAKEFLAGS macro. If it
# gives you any trouble, just delete the macro. It is used when recursively
# calling make (i.e. when rebuilding)
MKFLAGS= $(MFLAGS)$(MAKEFLAGS)

MAKEFILE_DIR= $(TI_DIR)\boards\DSK5509A_V1\examples\dsk_app_idle

# The active configuration can be one of these valid build configurations:
# all, Debug
ACTIVE_CONFIG= Debug

# These DIR_x macros store the directories of the files used in this project.
# There must be no trailing spaces after these macros.

DIR_1= $(TI_DIR)\plugins\bios

DIR_2= Debug

DIR_3= $(TI_CSLDIR)\include

DIR_4= $(TI_BIOSDIR)\include

DIR_5= $(TI_CGENDIR)\include

DIR_6= $(TI_CGENDIR)\bin

DIR_7= ..\..\include

SOURCE=aic23.c
SOURCE=dsk_app.c
SOURCE=dsk_app_idle.cdb
SOURCE=userlinker.cmd

active_config: $(ACTIVE_CONFIG)

norecurse: $(ACTIVE_CONFIG)_norecurse

clean: $(ACTIVE_CONFIG)clean

clean_norecurse: $(ACTIVE_CONFIG)clean_norecurse

rebuild: $(ACTIVE_CONFIG)rebuild

force_rebuild: 

all: Debug 

allclean: Debugclean 

allrebuild: Debugrebuild 


Debugclean: Debugclean_norecurse

Debugclean_norecurse: 
	-@del /F dsk_app_idlecfg.cmd
	-@del /F dsk_app_idlecfg.h
	-@del /F dsk_app_idlecfg.h55
	-@del /F dsk_app_idlecfg.s55
	-@del /F dsk_app_idlecfg_c.c
	-@del /F $(DIR_2)\aic23.obj
	-@del /F $(DIR_2)\dsk_app.obj
	-@del /F $(DIR_2)\dsk_app_idlecfg.obj
	-@del /F $(DIR_2)\dsk_app_idlecfg_c.obj
	-@del /F $(DIR_2)\dsk_app_idle.out

Debugrebuild: 
	$(MAKE) $(MFLAGS) -f makefile.file Debug FRC=force_rebuild

Debug: Debug_norecurse

Debug_norecurse: $(DIR_2)\dsk_app_idle.out



dsk_app_idlecfg.cmd \
dsk_app_idlecfg.h \
dsk_app_idlecfg.h55 \
dsk_app_idlecfg.s55 \
dsk_app_idlecfg_c.c: $(FRC) dsk_app_idle.cdb 
	"$(DIR_1)\gconfgen" dsk_app_idle.cdb

$(DIR_2)\aic23.obj: $(FRC) aic23.c aic23.h $(DIR_3)\csl.h $(DIR_3)\csl_i2c.h $(DIR_4)\std.h $(DIR_3)\_csl.h $(DIR_3)\csl_chiphal.h $(DIR_3)\csl_i2cdat.h $(DIR_3)\csl_i2chal.h $(DIR_3)\csl_csldat.h $(DIR_3)\csl_datasz.h $(DIR_3)\csl_err.h $(DIR_3)\csl_irq.h $(DIR_3)\csl_std.h $(DIR_3)\csl_stdhal.h $(DIR_3)\csl_cslhal.h $(DIR_3)\csl_bctdat.h $(DIR_3)\csl_chipdat.h $(DIR_3)\csl_datdat.h $(DIR_3)\csl_dmadat.h $(DIR_3)\csl_emifdat.h $(DIR_3)\csl_errdat.h $(DIR_3)\csl_gpiodat.h $(DIR_3)\csl_gptdat.h $(DIR_3)\csl_icachdat.h $(DIR_3)\csl_irqdat.h $(DIR_3)\csl_mcbspdat.h $(DIR_3)\csl_mmcdat.h $(DIR_3)\csl_plldat.h $(DIR_3)\csl_pwrdat.h $(DIR_3)\csl_rtcdat.h $(DIR_3)\csl_timdat.h $(DIR_3)\csl_uartdat.h $(DIR_3)\csl_wdtimdat.h $(DIR_3)\csl_irqhal.h $(DIR_3)\tistdtypes.h $(DIR_3)\csl_dmadatA.h $(DIR_3)\csl_dmadatB.h $(DIR_3)\csl_gpio5502dat.h $(DIR_3)\csl_gpio5509dat.h $(DIR_3)\csl_gpio5510dat.h $(DIR_3)\csl_time.h $(DIR_3)\_csl_gpiodat.h $(DIR_3)\_csl_pgpiodat.h $(DIR_5)\linkage.h 
	"$(DIR_6)\cl55" -g -mg -q -fr"./Debug" -i"." -i"../../include" -d"_DEBUG" -d"CHIP_5509A" -ml "aic23.c" 

$(DIR_2)\dsk_app.obj: $(FRC) dsk_app.c aic23.h $(DIR_3)\csl.h $(DIR_3)\csl_dma.h $(DIR_3)\csl_irq.h $(DIR_3)\csl_mcbsp.h $(DIR_3)\csl_pwr.h $(DIR_7)\dsk5509.h dsk_app_idlecfg.h $(DIR_4)\std.h $(DIR_3)\_csl.h $(DIR_3)\csl_dmahal.h $(DIR_3)\csl_irqdat.h $(DIR_3)\csl_irqhal.h $(DIR_3)\csl_mcbspdat.h $(DIR_3)\csl_mcbsphal.h $(DIR_3)\csl_pwrhal.h $(DIR_4)\hst.h $(DIR_4)\swi.h $(DIR_4)\tsk.h $(DIR_4)\log.h $(DIR_4)\sts.h $(DIR_3)\csl_chiphal.h $(DIR_3)\csl_csldat.h $(DIR_3)\csl_datasz.h $(DIR_3)\csl_err.h $(DIR_3)\csl_std.h $(DIR_3)\csl_stdhal.h $(DIR_3)\csl_cslhal.h $(DIR_3)\csl_bctdat.h $(DIR_3)\csl_chipdat.h $(DIR_3)\csl_datdat.h $(DIR_3)\csl_dmadat.h $(DIR_3)\csl_emifdat.h $(DIR_3)\csl_errdat.h $(DIR_3)\csl_gpiodat.h $(DIR_3)\csl_gptdat.h $(DIR_3)\csl_i2cdat.h $(DIR_3)\csl_icachdat.h $(DIR_3)\csl_mmcdat.h $(DIR_3)\csl_plldat.h $(DIR_3)\csl_pwrdat.h $(DIR_3)\csl_rtcdat.h $(DIR_3)\csl_timdat.h $(DIR_3)\csl_uartdat.h $(DIR_3)\csl_wdtimdat.h $(DIR_3)\tistdtypes.h $(DIR_3)\csl_dmadatA.h $(DIR_3)\csl_dmadatB.h $(DIR_3)\csl_gpio5502dat.h $(DIR_3)\csl_gpio5509dat.h $(DIR_3)\csl_gpio5510dat.h $(DIR_3)\csl_time.h $(DIR_3)\_csl_gpiodat.h $(DIR_3)\_csl_pgpiodat.h $(DIR_5)\linkage.h 
	"$(DIR_6)\cl55" -g -mg -q -fr"./Debug" -i"." -i"../../include" -d"_DEBUG" -d"CHIP_5509A" -ml "dsk_app.c" 

$(DIR_2)\dsk_app_idlecfg.obj: $(FRC) dsk_app_idlecfg.s55 dsk_app_idlecfg.h55 $(DIR_4)\confbeg.s55 $(DIR_4)\gbl.h55 $(DIR_4)\mem.h55 $(DIR_4)\obj.h55 $(DIR_4)\buf.h55 $(DIR_4)\clk.h55 $(DIR_4)\prd.h55 $(DIR_4)\rtdx.h55 $(DIR_4)\hst.h55 $(DIR_4)\hwi.h55 $(DIR_4)\swi.h55 $(DIR_4)\tsk.h55 $(DIR_4)\idl.h55 $(DIR_4)\isrc.h55 $(DIR_4)\log.h55 $(DIR_4)\pip.h55 $(DIR_4)\sem.h55 $(DIR_4)\mbx.h55 $(DIR_4)\que.h55 $(DIR_4)\lck.h55 $(DIR_4)\sio.h55 $(DIR_4)\sts.h55 $(DIR_4)\sys.h55 $(DIR_4)\gio.h55 $(DIR_4)\dev.h55 $(DIR_4)\udev.h55 $(DIR_4)\dgn.h55 $(DIR_4)\dhl.h55 $(DIR_4)\dpi.h55 $(DIR_4)\hook.h55 $(DIR_4)\dio.h55 $(DIR_4)\pwrm.h55 $(DIR_4)\confend.s55 
	"$(DIR_6)\cl55" -g -mg -q -fr"./Debug" -i"." -i"../../include" -d"_DEBUG" -d"CHIP_5509A" -ml "dsk_app_idlecfg.s55" 

$(DIR_2)\dsk_app_idlecfg_c.obj: $(FRC) dsk_app_idlecfg_c.c dsk_app_idlecfg.h $(DIR_4)\std.h $(DIR_4)\hst.h $(DIR_4)\swi.h $(DIR_4)\tsk.h $(DIR_4)\log.h $(DIR_4)\sts.h 
	"$(DIR_6)\cl55" -g -mg -q -fr"./Debug" -i"." -i"../../include" -d"_DEBUG" -d"CHIP_5509A" -ml "dsk_app_idlecfg_c.c" 

$(DIR_2)\dsk_app_idle.out: $(FRC) dsk_app_idlecfg.cmd $(DIR_2)\aic23.obj $(DIR_2)\dsk_app.obj $(DIR_2)\dsk_app_idlecfg.obj $(DIR_2)\dsk_app_idlecfg_c.obj userlinker.cmd 
	-@echo -z -q -c -o"./Debug/dsk_app_idle.out" -x -l"../../lib/dsk5509bsl.lib"> makefile.Debug.lkf
	-@echo "dsk_app_idlecfg.cmd">> makefile.Debug.lkf
	-@echo "$(DIR_2)\aic23.obj">> makefile.Debug.lkf
	-@echo "$(DIR_2)\dsk_app.obj">> makefile.Debug.lkf
	-@echo "$(DIR_2)\dsk_app_idlecfg.obj">> makefile.Debug.lkf
	-@echo "$(DIR_2)\dsk_app_idlecfg_c.obj">> makefile.Debug.lkf
	-@echo "userlinker.cmd">> makefile.Debug.lkf
	"$(DIR_6)\cl55" -@"makefile.Debug.lkf"
	-@del /F makefile.Debug.lkf