![]() |
![]() |
| AtaFileStruct | |
| AtaMMCState | Structure to hold the media ATA state values specific to MMCSD |
| AtaStateStruct | |
| CSL_AcClassStruct | AC Control Object structure |
| CSL_AcCtrlObject | USB AC Control Object structure |
| CSL_AcInitStructApp | Audio Class application data structure |
| CSL_AcLogicalUnit | Audio Class Logical unit structure |
| CSL_AcLunAttribApp | AC application Logical unit attribute structure |
| CSL_AcObject | USB Audio Class Object structure |
| CSL_AcRequestStruct | Audio Class control request structure |
| CSL_CdcClassStruct | CDC Control Object structure |
| CSL_CdcCtrlObject | CDC Control Object structure |
| CSL_CdcInitStructApp | CDC application data structure |
| CSL_CdcLineCoding | CDC line coding structure |
| CSL_CdcObject | CDC Mass Storage Object structure |
| CSL_Config | Configuration structure |
| CSL_DAT_ChannelObj | DAT channel object |
| CSL_DMA_ChannelObj | DMA channel object |
| CSL_DMA_Config | DMA configuration structure |
| CSL_GpioConfig | Config structure of GPIO. This is used to setup and get values of GPIO Registers using GPIO_config and GPIO_getConfig function |
| CSL_GpioObj | Structure parameters for GPIO Handle |
| CSL_GpioPinConfig | Input parameters for configuring a GPIO pin This is used to configure the direction and edge detection |
| CSL_GptObj | Object structure |
| CSL_I2cConfig | I2C Config structure |
| CSL_I2cIsrAddr | I2C callback pointer structure |
| CSL_I2cObj | I2C Object structure |
| CSL_I2cSetup | I2C Setup structure |
| CSL_I2sObj | Object structure |
| CSL_IRQ_Config | Config structure for INTC module |
| CSL_IRQ_Dispatch | INTC dispatch structure parameters |
| CSL_IrqDataObj | INTC Data object structure parameters |
| CSL_LcdcBaseAddress | This will have the base-address information for the peripheral instance |
| CSL_LcdcConfigDma | Configuration parameters for DMA engine |
| CSL_LcdcConfigLidd | Configuration parameters for LCDC in LIDD mode |
| CSL_LcdcContext | LCDC specific context information. Present implementation doesn't have any Context information |
| CSL_LcdcHwSetup | Input parameters for setting up LCD Controller Parameters used to put LCDC into useful state |
| CSL_LcdcLiddTiming | Timing parameters for LCDC in LIDD mode |
| CSL_LcdcObj | This object contains the reference to the instance of LCDC opened using the CSL_lcdcOpen() |
| CSL_LcdcParam | LCDC specific parameters. Present implementation doesn't have any specific parameters |
| CSL_MMCCallBackObj | Structure array of isr function for MMCSD |
| CSL_MMCCardCsdObj | CSD Information for MMC and SD card |
| CSL_MMCCardIdObj | Card identification object |
| CSL_MMCCardObj | Structure for card specific information |
| CSL_MMCCardXCsdObj | Structure for extra feature of MMC and SD Object |
| CSL_MMCConfig | MMC config structure for setting MMC/SD Control register |
| CSL_MMCControllerObj | Structure for card specific information |
| CSL_MMCSDCidStruct | Structure to store the CID Information for MMC and SD card |
| CSL_MmcsdCmd | Command structure for the card |
| CSL_MMCSDCsdStruct | Structure to store the CSD Information for MMC and SD card |
| CSL_MmcsdDmaConfig | DMA configuration structure for MMCSD module |
| CSL_MmcsdResponse | Response array received from the controller |
| CSL_MMCSetupNative | Structure to store the some default configuration for MMCSD controller |
| CSL_MscClassStruct | MSC Control Object structure |
| CSL_MscCtrlObject | MSC Control Object structure |
| CSL_MscInitStructApp | MSC application data structure |
| CSL_MscLogicalUnit | MSC Logical unit structure |
| CSL_MscLunAttribApp | MSC application Logical unit attribute structure |
| CSL_MscObject | MSC Mass Storage Object structure |
| CSL_MscRequestStruct | MSC control request structure |
| CSL_NandAsyncBank | Current Asynchronous NAND Bank configuration |
| CSL_NandAsyncCfg | Nand Async config structure |
| CSL_NandAsyncWaitCfg | Nand Async wait config structure |
| CSL_NandConfig | Nand Hw configuration structure |
| CSL_NandObj | This object contains the reference to the instance of nand device |
| CSL_RtcAlarm | RTC Alarm Time Structure. Contains the field of hour, minute, second and milli second for Alarm time |
| CSL_RtcConfig | RTC Config Structure |
| CSL_RtcDate | RTC Date Structure. Contains the field of year, month and day for Date |
| CSL_RtcIsrAddr | Declarations for interrupt routines |
| CSL_RtcIsrDispatchTable | Structure array of isr function for RTC |
| CSL_RtcTime | RTC Time Structure. Contains the field of hour, minute, second and milli second for time |
| CSL_SarChConfig | Structure parameters for SAR Register Configuration API |
| CSL_SarChSetup | Input parameters for setup API |
| CSL_SarHandleObj | Structure parameters for SAR handler |
| CSL_SdioCardObj | Structure for card specific information |
| CSL_SdioConfig | SDIo config structure for setting SDIO Control register |
| CSL_SdioControllerObj | Structure for card specific information |
| CSL_SdioResponse | Response array received from the controller |
| CSL_SpiObj | Object structure |
| CSL_UartConfig | UART Config structure The members of this structure directly maps to a particular register of UART |
| CSL_UartIsrAddr | UART callback pointer structure |
| CSL_UartObj | UART Object structure |
| CSL_UartSetup | UART Setup structure |
| CSL_UsbConfig | USB Config structure |
| CSL_UsbContext | USB context information structure |
| CSL_UsbDataStruct | USB data structure to send and receive data |
| CSL_UsbEpObj | Data Structure for USB Endpoint Object |
| CSL_UsbEpStatus | USB end point status structure |
| CSL_UsbHostBufDescr | USB DMA host buffer descriptor structure |
| CSL_UsbHostPktDescr | USB DMA host packet descriptor structure |
| CSL_UsbMsgObj | USB message object structure |
| CSL_UsbSetupStruct | Data structure to hold USB setup packet |
| CSL_UsbTransfer | USB end point transfer data structure |
| CSL_WdtObj | Object structure |
| I2S_Config | Configuration structure |
| PLL_Config | Config-structure |
| PLL_Obj | This object contains the reference to the instance of pll device |
| SPI_Config | Configuration structure |
| WDTIM_Config | Configuration structure |
1.7.4