![]() |
![]() |
USB CDC functional layer API source file. More...
Functions | |
| CSL_Status | CDC_Open (pCdcAppClassHandle pAppClassHandle) |
| CSL_Status | CDC_OpenFullspeed (pCdcAppClassHandle pAppClassHandle) |
| static CSL_Status | CDC_Setup (pCdcAppClassHandle pAppClassHandle, Bool usbSpeedCfg) |
| CSL_Status | CDC_Close (pCdcAppClassHandle pAppClassHandle) |
| Uint16 | CDC_GetactivityFlagStatus (void *pCDC) |
| Uint16 | CDC_GetsuspendFlagStatus (void *pCDC) |
| CSL_CdcRequestRet | CDC_eventHandler (pUsbContext pContext, CSL_CdcClassStruct *hCdcClass) |
| CSL_Status | CDC_bulkOutHandler (pUsbContext pContext, CSL_CdcInitStructApp *cdcAppHandle) |
| CSL_Status | CDC_bulkInHandler (pUsbContext pContext, CSL_CdcInitStructApp *cdcAppHandle) |
| Uint16 | CDC_getData (pUsbContext pContext, CSL_CdcInitStructApp *cdcAppHandle, Uint16 *data) |
| Uint16 | CDC_putData (pUsbContext pContext, CSL_CdcInitStructApp *cdcAppHandle, Uint16 *data, Uint16 size) |
USB CDC functional layer API source file.
Path: \(CSLPATH)\ src
| static CSL_Status CDC_Setup | ( | pCdcAppClassHandle | pAppClassHandle, |
| Bool | usbSpeedCfg | ||
| ) | [static] |
============================================================================
CDC_Setup
Description
This function used to setup the Cdc and Ctrl handles. This is an internal function and is called from CDC_Open or CDC_OpenFullspeed functions.
Arguments
pAppClassHandle Application handle to the CDC Class Obj
usbSpeedCfg USB speed selection parameter
0 - USB CDC operates in fullspeed mode
1 - USB CDC operates in highspeed mode
Return Value CSL_Status
Pre Condition
None
Post Condition
Initializes Cdc and Ctrl handles
Modifies
Cdc and Ctrl handle data
Example
CSL_CdcInitStructApp cdcAppHandle;
pCdcAppClassHandle pAppClassHandle;
Uint16 cdcAppBuffer[420];
CSL_Status status;
pAppClassHandle = &cdcAppHandle;
// Assign values to all the members in cdcAppHandle struct
cdcAppHandle.pCdcObj = &cdcAppBuffer[0];
.....
.....
// Setup USB for highspeed
status = CDC_Setup(pAppClassHandle, TRUE);
============================================================================
References CSL_CdcInitStructApp::bulkHandler, CSL_CdcObject::bulkInEpObj, CSL_CdcObject::bulkOutEpObj, CSL_CdcClassStruct::cdcHandle, CSL_CDC_INTR_IN_EP, CSL_USB_BULK, CSL_USB_CTRL, CSL_USB_EP0_PACKET_SIZE, CSL_USB_EP1_PACKET_SIZE_FS, CSL_USB_EP1_PACKET_SIZE_HS, CSL_USB_EVENT_EOT, CSL_USB_EVENT_RESET, CSL_USB_EVENT_RESUME, CSL_USB_EVENT_SETUP, CSL_USB_EVENT_SUSPEND, CSL_USB_IN_EP0, CSL_USB_INTR, CSL_USB_OUT_EP0, CSL_CdcClassStruct::ctrlHandle, CSL_CdcInitStructApp::ctrlHandler, CSL_CdcCtrlObject::ctrlInEpObj, CSL_CdcCtrlObject::ctrlOutEpObj, CSL_CdcCtrlObject::curConfigStat, CSL_CdcCtrlObject::devNum, CSL_CdcCtrlObject::hEpObjArray, CSL_CdcInitStructApp::intrHandler, CSL_CdcObject::intrInEpObj, CSL_CdcObject::intrOutEpObj, CSL_CdcInitStructApp::pCdcObj, CSL_CdcCtrlObject::suspendFlag, USB_connectDev(), USB_initEndptObj(), USB_setParams(), and CSL_CdcCtrlObject::usbSpeedCfg.
Referenced by CDC_Open(), and CDC_OpenFullspeed().
1.7.4