![]() |
![]() |
Functional layer API source file for MMCSD ATA file system interface. More...
Defines | |
| #define | ENABLE_CACHE 1 |
Functions | |
| AtaError | MMC_initState (AtaState *pDrive) |
| AtaError | MMC_readWriteControl (AtaSector phySector, void *pAtaMediaState, AtaUint16 *pWord, int last_sector) |
| AtaError | MMC_issueReadCommand (AtaSector phySector, void *pAtaMediaState, AtaUint16 sectorCount) |
| AtaError | MMC_readNextWord (void *pAtaMediaState, AtaUint16 *pWord) |
| AtaError | MMC_readNextWord1 (void *pAtaMediaState, AtaUint16 *pWord, AtaUint16 word_delta) |
| AtaError | MMC_readNextNWords (void *pAtaMediaState, AtaUint16 *pData, AtaUint16 words) |
| AtaError | MMC_writeSector (AtaSector phySector, void *pAtaMediaState, AtaUint16 *pWord, int byteSwap) |
| AtaError | MMC_readNSectors (void *pAtaMediaState, AtaUint16 *pReadBuf, AtaSector startSector, AtaUint16 sectorCount) |
| AtaError | MMC_writeNSectors (void *pAtaMediaState, AtaUint16 *pWriteBuf, AtaSector startSector, AtaUint16 sectorCount) |
| AtaError | MMC_read_CID (void *pAtaMediaState, unsigned int *pBuf) |
| AtaError | MMC_read_CSD (void *pAtaMediaState, unsigned int *pBuf) |
| AtaError | MMC_writeSectorFlush (void *pAtaMediaState) |
| int | MMC_commandReadyStatusCheck (void *pAtaMediaState) |
| AtaError | MMC_dataReadyStatusCheck (void *pAtaMediaState) |
| AtaError | MMC_busyStatusCheck (void *pAtaMediaState) |
| AtaUint16 | MMC_getSerialID (void *pAtaMediaState, AtaSerialID *pSerID) |
| AtaUint16 | MMC_file_system_format (void *pAtaMediaState) |
| AtaError | MMC_reset (void *pAtaMediaState) |
| AtaUint16 | MMC_get_time (void) |
| AtaUint16 | MMC_get_mod_time (void) |
| AtaUint16 | MMC_get_date (void) |
| AtaUint16 | MMC_get_mod_date (void) |
| AtaError | MMC_flushFat (void *pAtaMediaState) |
| static AtaError | getAtaErrorNo (CSL_Status result) |
Variables | |
| Uint16 | gReadBuf [CSL_MMCSD_PAGE_SIZE/2] = {0xbb,} |
| Uint16 | gWordCount = 256 |
| AtaSector | gNextPhySector = 0 |
| Uint16 | gWriteBuf [2 *CSL_MMCSD_PAGE_SIZE] |
| AtaSector | cached_phySector0 |
| AtaSector | cached_phySector1 |
| AtaSector | cached_phySector2 |
| AtaSector | cached_phySector3 |
| AtaUint16 | nbuf_cached = 0 |
Functional layer API source file for MMCSD ATA file system interface.
Path: \(CSLPATH)\ src
| static AtaError getAtaErrorNo | ( | CSL_Status | result | ) | [static] |
===========================================================================
getAtaErrorNo
Description
This function checks the return value send by the MMCSD CSL module and returns the corresponding error value to the ATA File system. This function is called in case of any error occurred
Arguments
result Result returned by the CSL MMCSD module
Return Value AtaError
Pre Condition
None
Post Condition
Returns ATA Error codes
Modifies
None
Example
CSL_Status result;
AtaError ataErr;
result = MMC_init();
ataErr = getAtaErrorNo(result);
===========================================================================
Referenced by MMC_issueReadCommand(), MMC_readNSectors(), MMC_writeNSectors(), and MMC_writeSector().
| AtaError MMC_readWriteControl | ( | AtaSector | phySector, |
| void * | pAtaMediaState, | ||
| AtaUint16 * | pWord, | ||
| int | last_sector | ||
| ) |
===========================================================================
MMC_readWriteControl //KR041110
Description
This function is used to cache and write data to the media. This function can write 1 to 4 sectors each sector containing 512 bytes
Arguments
phySector Sector number from which data needs to be read
pAtaMediaState ATA media state structure
pWord Write data buffer
last_sector Flag to flush cache
Return Value AtaError
Pre Condition
MMC_initState API should be called successfully.
Post Condition
Writes Data to MMC/SD card
Modifies
MMCSD Sector data
Example
#define CSL_MMCSD_BUF_SIZE (256u)
AtaMMCState ataMediaState;
AtaState ataState;
AtaState *pAtaState;
AtaError ataErr;
AtaSector phySector;
AtaUint16 writeBuf[CSL_MMCSD_BUF_SIZE];
pAtaState = &ataState;
phySector = 0;
ataState->pAtaMediaState = &ataMediaState;
ataErr = MMC_initState(&ataState);
ataErr = pAtaState->AtaWriteSector(phySector,
ataState->pAtaMediaState,
writeBuf, FALSE);
===========================================================================
References CSL_MMCSD_PAGE_SIZE, MMC_writeNSectors(), and MMC_writeSector().
Referenced by MMC_initState().
1.7.4