![]() |
![]() |
Functional layer API header file for MMCSD ATA file system interface. More...
Go to the source code of this file.
Data Structures | |
| struct | AtaMMCState |
| Structure to hold the media ATA state values specific to MMCSD. More... | |
Defines | |
| #define | CSL_MMCSD_PAGE_SIZE (512u) |
| #define | USE_ATA_NO_SWAP (TRUE) |
Typedefs | |
| typedef struct AtaMMCState | AtaMMCState |
| Structure to hold the media ATA state values specific to MMCSD. | |
Functions | |
| AtaError | MMC_readWriteControl (AtaSector phySector, void *pAtaMediaState, AtaUint16 *pWord, int byteSwap) |
| AtaError | MMC_initState (AtaState *pDrive) |
| AtaError | MMC_issueReadCommand (AtaSector phySector, void *pAtaMediaState, AtaUint16 sectorCount) |
| AtaError | MMC_readNextWord (void *pAtaMediaState, AtaUint16 *pWord) |
| AtaError | MMC_readNextWord1 (void *pAtaMediaState, AtaUint16 *pWord, AtaUint16 word_delta) |
| AtaError | MMC_readNextNWords (void *pAtaMediaState, AtaUint16 *pData, AtaUint16 words) |
| AtaError | MMC_writeSector (AtaSector phySector, void *pAtaMediaState, AtaUint16 *pWord, int byteSwap) |
| AtaError | MMC_readNSectors (void *pAtaMediaState, AtaUint16 *pReadBuf, AtaSector startSector, AtaUint16 sectorCount) |
| AtaError | MMC_writeNSectors (void *pAtaMediaState, AtaUint16 *pWriteBuf, AtaSector startSector, AtaUint16 sectorCount) |
| AtaError | MMC_read_CID (void *pAtaMediaState, unsigned int *pBuf) |
| AtaError | MMC_read_CSD (void *pAtaMediaState, unsigned int *pBuf) |
| AtaError | MMC_writeSectorFlush (void *pAtaMediaState) |
| int | MMC_commandReadyStatusCheck (void *pAtaMediaState) |
| AtaError | MMC_dataReadyStatusCheck (void *pAtaMediaState) |
| AtaError | MMC_busyStatusCheck (void *pAtaMediaState) |
| AtaUint16 | MMC_getSerialID (void *pAtaMediaState, AtaSerialID *pSerID) |
| AtaUint16 | MMC_file_system_format (void *pAtaMediaState) |
| AtaError | MMC_reset (void *pAtaMediaState) |
| AtaUint16 | MMC_get_time (void) |
| AtaUint16 | MMC_get_mod_time (void) |
| AtaUint16 | MMC_get_date (void) |
| AtaUint16 | MMC_get_mod_date (void) |
| AtaError | MMC_flushFat (void *pAtaMediaState) |
| static AtaError | getAtaErrorNo (CSL_Status result) |
Functional layer API header file for MMCSD ATA file system interface.
Path: \(CSLPATH)\ inc
| AtaError MMC_readWriteControl | ( | AtaSector | phySector, |
| void * | pAtaMediaState, | ||
| AtaUint16 * | pWord, | ||
| int | last_sector | ||
| ) |
===========================================================================
MMC_readWriteControl //KR041110
Description
This function is used to cache and write data to the media. This function can write 1 to 4 sectors each sector containing 512 bytes
Arguments
phySector Sector number from which data needs to be read
pAtaMediaState ATA media state structure
pWord Write data buffer
last_sector Flag to flush cache
Return Value AtaError
Pre Condition
MMC_initState API should be called successfully.
Post Condition
Writes Data to MMC/SD card
Modifies
MMCSD Sector data
Example
#define CSL_MMCSD_BUF_SIZE (256u)
AtaMMCState ataMediaState;
AtaState ataState;
AtaState *pAtaState;
AtaError ataErr;
AtaSector phySector;
AtaUint16 writeBuf[CSL_MMCSD_BUF_SIZE];
pAtaState = &ataState;
phySector = 0;
ataState->pAtaMediaState = &ataMediaState;
ataErr = MMC_initState(&ataState);
ataErr = pAtaState->AtaWriteSector(phySector,
ataState->pAtaMediaState,
writeBuf, FALSE);
===========================================================================
References CSL_MMCSD_PAGE_SIZE, MMC_writeNSectors(), and MMC_writeSector().
Referenced by MMC_initState().
1.7.4