![]() |
![]() |
SPI functional layer API defenition file. More...
#include "csl_spi.h"Functions | |
| CSL_Status | SPI_init (void) |
| CSL_SpiHandle | SPI_open (SPI_HwMode csNum, SPI_OperMode opMode) |
| CSL_Status | SPI_close (CSL_SpiHandle hSpi) |
| CSL_Status | SPI_config (CSL_SpiHandle hSpi, SPI_Config *spiHwConfig) |
| CSL_Status | SPI_deInit (void) |
| CSL_Status | SPI_read (CSL_SpiHandle hSpi, Uint16 *readBuffer, Uint16 bufLen) |
| CSL_Status | SPI_write (CSL_SpiHandle hSpi, Uint16 *writeBuffer, Uint16 bufLen) |
| CSL_Status | SPI_dataTransaction (CSL_SpiHandle hSpi, Uint16 *rwBuffer, Uint16 rwBufLen, SPI_Command readOrWrite) |
SPI functional layer API defenition file.
Path: \(CSLPATH)/src
1.7.4