CSL standard types definition file.
More...
#include <tistdtypes.h>
Go to the source code of this file.
Defines |
|
#define | TRUE ((Bool) 1) |
|
#define | FALSE ((Bool) 0) |
|
#define | NULL ((void*)0) |
Typedefs |
|
typedef Int16 | CSL_Uid |
|
typedef Int16 | CSL_ModuleId |
|
typedef Uint32 | CSL_Xio |
|
typedef Uint8 | CSL_BitMask8 |
|
typedef Uint16 | CSL_BitMask16 |
|
typedef Uint32 | CSL_BitMask32 |
|
typedef volatile Uint8 | CSL_Reg8 |
|
typedef volatile Uint16 | CSL_Reg16 |
|
typedef volatile Uint32 | CSL_Reg32 |
|
typedef Int16 | CSL_Status |
|
typedef Int16 | CSL_InstNum |
|
typedef Int16 | CSL_ChaNum |
|
typedef unsigned long long int | CSL_Uint64 |
|
typedef volatile unsigned int | CSL_VUint32 |
|
typedef volatile unsigned short | CSL_VUint16 |
|
typedef volatile unsigned char | CSL_VUint8 |
|
typedef Uint8 | BYTE |
|
typedef Uint8 * | PBYTE |
|
typedef Uint16 | WORD |
|
typedef Uint16 * | PWORD |
|
typedef Uint32 | DWORD |
|
typedef Uint32 * | PDWORD |
|
typedef void * | PVOID |
|
typedef void | VOID |
|
typedef Bool * | PBool |
Enumerations |
| enum | CSL_OpenMode {
CSL_EXCLUSIVE = 0,
CSL_SHARED = 1
} |
| enum | CSL_Test {
CSL_FAIL = 0,
CSL_PASS = 1
} |
Detailed Description
CSL standard types definition file.
Path: \(CSLPATH)