Data Structures | Typedefs
GPIO Data Structures
GPIO

Data Structures

struct  CSL_GpioConfig
 Config structure of GPIO. This is used to setup and get values of GPIO Registers using GPIO_config and GPIO_getConfig function. More...
struct  CSL_GpioPinConfig
 Input parameters for configuring a GPIO pin This is used to configure the direction and edge detection. More...
struct  CSL_GpioObj
 structure parameters for GPIO Handle More...

Typedefs

typedef CSL_GpioObjGPIO_Handle
 this is a pointer to CSL_GpioObj and is passed as the first parameter to all GPIO CSL APIs