![]() |
![]() |
Data Structures | |
| struct | CSL_NandAsyncWaitCfg |
| Nand Async wait config structure. More... | |
| struct | CSL_NandAsyncCfg |
| Nand Async config structure. More... | |
| struct | CSL_NandAsyncBank |
| Current Asynchronous NAND Bank configuration. More... | |
| struct | CSL_NandConfig |
| Nand Hw configuration structure. More... | |
| struct | CSL_NandObj |
| This object contains the reference to the instance of nand device. More... | |
Typedefs | |
| typedef struct CSL_NandAsyncWaitCfg | CSL_NandAsyncWaitCfg |
| Nand Async wait config structure. | |
| typedef struct CSL_NandAsyncCfg | CSL_NandAsyncCfg |
| Nand Async config structure. | |
| typedef struct CSL_NandAsyncBank | CSL_NandAsyncBank |
| Current Asynchronous NAND Bank configuration. | |
| typedef struct CSL_NandConfig | CSL_NandConfig |
| Nand Hw configuration structure. | |
| typedef struct CSL_NandObj | CSL_NandObj |
| This object contains the reference to the instance of nand device. | |
| typedef CSL_NandObj * | CSL_NandHandle |
| Nand object structure pointer. | |
| typedef struct CSL_NandObj CSL_NandObj |
This object contains the reference to the instance of nand device.
This object is initialized during nand initialization and passed as the parameter to all nand CSL APIs
1.7.4