![]() |
![]() |
AC application Logical unit attribute structure. More...
#include <csl_audioClass.h>
Data Fields | |
| Uint32 | lbaSizeApp |
| Logical Block Size (size of each LB) | |
| Uint32 | mediaSizeApp |
| Total Number Of LB in the Media. | |
| Uint16 | removeableApp |
| Removable or Non removable Media. | |
| Uint16 | scsiInquiryConfData [CSL_AC_SCSI_INQUIRY_CONF_LEN] |
| SCSI Inquiry Data - User Configurable Items. | |
| Uint16 | mediaStateApp |
| Media State. | |
| Uint16 | readwriteApp |
| Device is Readable and/or Writable. | |
AC application Logical unit attribute structure.
Holds the attributes of every logical unit. This structure should be filled by the application.
1.7.4