Data Fields
CSL_LcdcLiddTiming Struct Reference

Timing parameters for LCDC in LIDD mode. More...

#include <csl_lcdc.h>

Data Fields

Uint16 wSu
Uint16 wStrobe
Uint16 wHold
Uint16 rSu
Uint16 rStrobe
Uint16 rHold
Uint16 ta

Detailed Description

Timing parameters for LCDC in LIDD mode.

Used to configure timing parameters in LIDD mode


Field Documentation

Read Strobe Hold cycles (0-15)

Read Strobe Duration cycles (0-63)

Read Strobe Set-Up cycles (0-31)

Turn Around cycles (0-3)

Write Strobe Hold cycles (0-15)

Write Strobe Duration cycles (0-63)

Write Strobe Set-Up cycles (0-31)


The documentation for this struct was generated from the following file: