![]() |
![]() |
Command structure for the card. More...
#include <csl_mmcsd.h>
Data Fields | |
| Uint16 | idx |
| CSL_MmcsdRespType | respType |
| CSL_MmcsdRespBusy | busy |
| CSL_MmcsdCmdType | type |
| CSL_MmcsdDir | dir |
| CSL_MmcsdLineChr | lineChr |
Command structure for the card.
This structure has parameters that is used to send a command to the MMC/SD device.
Response property with respect to busy signal
Direction for the data incase of data transferred involved
| Uint16 CSL_MmcsdCmd::idx |
Index of the command
Line characteristics of the command
Response expected for the command
Protocol type of the command
1.7.4