Data Fields
CSL_RtcAlarm Struct Reference

RTC Alarm Time Structure. Contains the field of hour, minute, second and milli second for Alarm time. More...

#include <csl_rtc.h>

Data Fields

Uint16 year
Uint16 month
Uint16 day
Uint16 hours
Uint16 mins
Uint16 secs
Uint16 mSecs

Detailed Description

RTC Alarm Time Structure. Contains the field of hour, minute, second and milli second for Alarm time.


Field Documentation

Day Alarm field value between 1 - 31

Hour Alarm field value between 0 - 23

Minute Alarm field value between 0 - 59

Month Alarm field value between 1 - 12

MSecond Alarm field value between 0 - 1023

Second Alarm field value between 0 - 59

Year Alarm field value between 0 - 99


The documentation for this struct was generated from the following file: