Data Fields
CSL_UsbHostPktDescr Struct Reference

USB DMA host packet descriptor structure. More...

#include <csl_usb.h>

Data Fields

volatile Uint32 PacketInfoWord0
 DMA packet information word 0.
volatile Uint32 PacketInfoWord1
 DMA packet information word 1.
volatile Uint32 PacketInfoWord2
 DMA packet information word 2.
volatile Uint32 Buffer0InfoWord0
 DMA buffer0 information word 0.
volatile Uint32 Buffer0InfoWord1
 DMA buffer0 information word 1.
volatile Uint32 LinkingWord
 Linking word to the next packet.
volatile Uint32 OriginalBuffer0InfoWord0
 DMA Original buffer0 information word 0.
volatile Uint32 OriginalBuffer0InfoWord1
 DMA Original buffer0 information word 1.

Detailed Description

USB DMA host packet descriptor structure.


The documentation for this struct was generated from the following file: