Data Fields
CSL_UsbSetupStruct Struct Reference

Data structure to hold USB setup packet. More...

#include <csl_usb.h>

Data Fields

int newPacket
 new = 1, structure holds new setup packet
Uint16 bmRequestType
 Byte 0 of setup packet.
Uint16 bRequest
 Byte 1 of setup packet.
Uint16 wValue
 Byte 2 and 3 of setup packet.
Uint16 wIndex
 Byte 4 and 5 setup packet.
Uint16 wLength
 Byte 6 and 7 of setup packet.

Detailed Description

Data structure to hold USB setup packet.


The documentation for this struct was generated from the following file: