C55XX CSL EXAMPLE
CSL WDT EXAMPLE DOCUMENTATION

WDT EXAMPLE - CPU RESET TEST

TEST DESCRIPTION:

This example code verifies the functionality of watchdog timer of the C5505/C5515 DSP. Watchdog timer functionality is to prevent the system from locking up if the software becomes trapped in loops with no controlled exit. To determine that the software is operating properly, the watchdog timer requires a special service sequence to be executed periodically. Without this periodic servicing, the watchdog timer counter reaches zero and times out. Consequently, an active low pulse will be asserted on the watchdog output that is connected to the local hardware reset. Thus, forcing a reset of the CPU.

This test code configures the CSL WDT module and start the timer. Timer is serviced for 256 times to verify whether the timer is running properly. Each time the timer is serviced the timer counter should be reset and timer should re-start the counting. Timer count is read and displayed on the CCS "Stdout" window after servicing the counter. After servicing the counter for 256 times test code will stop servicing the timer and keeps reading and displaying the timer count. Timer count will go on decreasing and CPU will be reset when timer count reaches to zero. After CPU reset test code stops running and target will be disconnected.

NOTE: THIS TEST HAS BEEN DEVELOPED TO WORK WITH CHIP VERSIONS C5505 AND C5515. MAKE SURE THAT PROPER CHIP VERSION MACRO IS DEFINED IN THE FILE c55xx_csl\inc\csl_general.h.

TEST PROCEDURE:

TEST RESULT: